ProfileTransitionBuilderMisalignedModeType Enumeration¶
NXOpen.Features.ShipDesign.ProfileTransitionBuilder.MisalignedModeType is an alias for NXOpen.Features.ShipDesign.ProfileTransitionBuilderMisalignedModeType
-
class
NXOpen.Features.ShipDesign.
ProfileTransitionBuilderMisalignedModeType
¶ Bases:
object
Represents the misaligned profile mode.
Enum Members
Enum Member Enum Member Description NotAllowed Ignore misaligned profiles. ToBoundary Transition target directly to boundary end. Bisect Extend/trim boundary end to bisector plane between target and boundary. Transition target to new boundary end. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-