PlateChamferBuilderOffsetMethod Enumeration¶
NXOpen.Features.ShipDesign.PlateChamferBuilder.OffsetMethod is an alias for NXOpen.Features.ShipDesign.PlateChamferBuilderOffsetMethod
-
class
NXOpen.Features.ShipDesign.
PlateChamferBuilderOffsetMethod
¶ Bases:
object
The option to specify the method for chamfer offset method.
Enum Members
Enum Member Enum Member Description Depth Use depth parameter to define ramp RestDepth Use rest depth to define ramp ThinnerPlate Use the thickness of the thinner plate to define ramp depth -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-