PenetrationReviewRequestBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
PenetrationReviewRequestBuilder
¶ Bases:
NXOpen.Builder
Represents a
Features.ShipDesign.PenetrationRequest
builderTo create a new instance of this class, use
NXOpen.Features.ShipDesign.PenetrationRequestCollection.CreatePenetrationReviewRequestBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DueDate | Returns or sets the due date |
ReviewDecisions | Returns or sets the review decisions |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMultilineStringComments | Returns the multiline string comments |
GetObject | Returns the object currently being edited by this builder. |
SetMultilineStringComments | Sets the multiline string comments |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DueDate¶
-
PenetrationReviewRequestBuilder.
DueDate
¶ Returns or sets the due date
-------------------------------------
Getter Method
Signature
DueDate
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DueDate
Parameters: stringDueDate (str) – New in version NX8.0.0.
License requirements: nx_penetration_mgmt (“Penetration Management”)
ReviewDecisions¶
-
PenetrationReviewRequestBuilder.
ReviewDecisions
¶ Returns or sets the review decisions
-------------------------------------
Getter Method
Signature
ReviewDecisions
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReviewDecisions
Parameters: enumReviewDecisions (int) – New in version NX8.0.0.
License requirements: nx_penetration_mgmt (“Penetration Management”)
Method Detail¶
GetMultilineStringComments¶
-
PenetrationReviewRequestBuilder.
GetMultilineStringComments
¶ Returns the multiline string comments
Signature
GetMultilineStringComments()
Returns: Return type: list of str New in version NX8.0.0.
License requirements: None.
SetMultilineStringComments¶
-
PenetrationReviewRequestBuilder.
SetMultilineStringComments
¶ Sets the multiline string comments
Signature
SetMultilineStringComments(multilineStringComments)
Parameters: multilineStringComments (list of str) – New in version NX8.0.0.
License requirements: nx_penetration_mgmt (“Penetration Management”)
Validate¶
-
PenetrationReviewRequestBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.