PenetrationRequestRequestType Enumeration

NXOpen.Features.ShipDesign.PenetrationRequest.RequestType is an alias for NXOpen.Features.ShipDesign.PenetrationRequestRequestType

class NXOpen.Features.ShipDesign.PenetrationRequestRequestType

Bases: object

Represents the request type

Enum Members

Enum Member Enum Member Description
Single
Multiple
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.