PenetrationManager Class¶
-
class
NXOpen.Features.ShipDesign.
PenetrationManager
¶ Bases:
object
Contains the collection objects for creating and iterating over Penetration Request Properties objects.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX7.5.1.
“PenetrationUtils”, “Returns the PenetrationUtils instance ” “PenetrationRequestCollection”, “Returns the PenetrationRequestCollection instance “
PenetrationUtils¶
-
PenetrationManager.
PenetrationUtils
¶ Returns the PenetrationUtils instance
Signature
PenetrationUtils
New in version NX8.0.0.
Returns: Return type: NXOpen.Features.ShipDesign.PenetrationUtils
PenetrationRequestCollection¶
-
PenetrationManager.
PenetrationRequestCollection
¶ Returns the PenetrationRequestCollection instance
Signature
PenetrationRequestCollection
New in version NX8.0.0.
Returns: Return type: NXOpen.Features.ShipDesign.PenetrationRequestCollection