OrientationPointMethodsBuilderMeasureAlongTypes Enumeration¶
NXOpen.Features.ShipDesign.OrientationPointMethodsBuilder.MeasureAlongTypes is an alias for NXOpen.Features.ShipDesign.OrientationPointMethodsBuilderMeasureAlongTypes
-
class
NXOpen.Features.ShipDesign.
OrientationPointMethodsBuilderMeasureAlongTypes
¶ Bases:
object
Settings to indicate how the distance is measured.
Enum Members
Enum Member Enum Member Description Curve The distance is measured along the landing curve. Axis The distance is measured along the orthogonal direction closest to the landing curve tangent direction. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-