OrientationDefinitionBuilderPlacementSideTypes Enumeration¶
NXOpen.Features.ShipDesign.OrientationDefinitionBuilder.PlacementSideTypes is an alias for NXOpen.Features.ShipDesign.OrientationDefinitionBuilderPlacementSideTypes
-
class
NXOpen.Features.ShipDesign.
OrientationDefinitionBuilderPlacementSideTypes
¶ Bases:
object
Settings to indicate which side of the placement faces the stiffener is to be placed.
Enum Members
Enum Member Enum Member Description SameAsNormal The stiffener will be placed on the positive normal side of the placement faces. OppositeNormal The stiffener will be placed on the negative normal side of the placement faces. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-