OrientationAngleMethodsBuilderMethodTypes Enumeration

NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilder.MethodTypes is an alias for NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderMethodTypes

class NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderMethodTypes

Bases: object

Settings used to determine how the angle is defined.

Enum Members

Enum Member Enum Member Description
Angle Angle is defined by specifying a constant angle from a reference object.
Vector Angle is defined by specifying a vector to align with.
Aligned Angle is the same as the previous or following region.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.