OrientationAngleMethodsBuilderAlignAtTypes Enumeration¶
NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilder.AlignAtTypes is an alias for NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderAlignAtTypes
-
class
NXOpen.Features.ShipDesign.
OrientationAngleMethodsBuilderAlignAtTypes
¶ Bases:
object
Is the angle to be aligned with the region adjacent to start of this region or adjacent to the end of this region. Note the Start setting cannot be used for the first region, and the End setting cannot be used for the last region.
Enum Members
Enum Member Enum Member Description Start End -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-