MirrorShipStructureBuilderMirrorApproach Enumeration¶
NXOpen.Features.ShipDesign.MirrorShipStructureBuilder.MirrorApproach is an alias for NXOpen.Features.ShipDesign.MirrorShipStructureBuilderMirrorApproach
-
class
NXOpen.Features.ShipDesign.
MirrorShipStructureBuilderMirrorApproach
¶ Bases:
object
Represents the approach of mirroring ship standard parts.
Enum Members
Enum Member Enum Member Description CreateLinkedMirrorBody The approach by creating linked mirror body. CopySourceFeaturesAndReparent The approach by copy source features and reparenting. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-