ManufacturingStockBuilderStockDataSourceType Enumeration¶
NXOpen.Features.ShipDesign.ManufacturingStockBuilder.StockDataSourceType is an alias for NXOpen.Features.ShipDesign.ManufacturingStockBuilderStockDataSourceType
-
class
NXOpen.Features.ShipDesign.
ManufacturingStockBuilderStockDataSourceType
¶ Bases:
object
the data source from which the intial manufacturing data will be read.
Enum Members
Enum Member Enum Member Description NotSet Set to None if we edit this feature CustomerDefault Initial data will be read from the customer default -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-