ManufacturingStockBuilderObjectType Enumeration¶
NXOpen.Features.ShipDesign.ManufacturingStockBuilder.ObjectType is an alias for NXOpen.Features.ShipDesign.ManufacturingStockBuilderObjectType
-
class
NXOpen.Features.ShipDesign.
ManufacturingStockBuilderObjectType
¶ Bases:
object
the object to which the manufacturing attributes will be written.
Enum Members
Enum Member Enum Member Description NotSet None Edge Edge Face Face Body Body Feature Feature Part Part Num Total Object Num -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-