ManufacturingStockBuilderLockedStatus Enumeration¶
NXOpen.Features.ShipDesign.ManufacturingStockBuilder.LockedStatus is an alias for NXOpen.Features.ShipDesign.ManufacturingStockBuilderLockedStatus
-
class
NXOpen.Features.ShipDesign.
ManufacturingStockBuilderLockedStatus
¶ Bases:
object
the NX attribute locked status.
Enum Members
Enum Member Enum Member Description Unlocked The NX attribute is set with unlocked status. Locked The NX attribute is set with locked status. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-