ManufacturingStockBuilderCheckBoxStatus Enumeration¶
NXOpen.Features.ShipDesign.ManufacturingStockBuilder.CheckBoxStatus is an alias for NXOpen.Features.ShipDesign.ManufacturingStockBuilderCheckBoxStatus
-
class
NXOpen.Features.ShipDesign.
ManufacturingStockBuilderCheckBoxStatus
¶ Bases:
object
the check box status.
Enum Members
Enum Member Enum Member Description Unchecked Unchecked Checked Checked Required Checked and Cannot be modified -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-