ManufacturingAssemblyNavigatorBuilderOrientationType Enumeration¶
NXOpen.Features.ShipDesign.ManufacturingAssemblyNavigatorBuilder.OrientationType is an alias for NXOpen.Features.ShipDesign.ManufacturingAssemblyNavigatorBuilderOrientationType
-
class
NXOpen.Features.ShipDesign.
ManufacturingAssemblyNavigatorBuilderOrientationType
¶ Bases:
object
Container Orientation Types
Enum Members
Enum Member Enum Member Description Aft Aft Orientation Starboard Starboard Orientation Up Up Orientation Forward Forward Orientation Port Port Orientation Down Down Orientation Custom Custom Orientation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-