LongitudinalBulkheadBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.LongitudinalBulkheadBuilder.Types is an alias for NXOpen.Features.ShipDesign.LongitudinalBulkheadBuilderTypes
-
class
NXOpen.Features.ShipDesign.
LongitudinalBulkheadBuilderTypes
¶ Bases:
object
Indicates the method that is being used to define the mold face of the longitudinal bulkhead.
Enum Members
Enum Member Enum Member Description SheetBody Mold face is being defined by a selected sheet body. Planes Mold face is being defined by selected or defined planes. Extrusion Mold face is being defined by extruding a supplied section shape. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-