InverseBendingLinesBuilderReferencePlaneType Enumeration¶
NXOpen.Features.ShipDesign.InverseBendingLinesBuilder.ReferencePlaneType is an alias for NXOpen.Features.ShipDesign.InverseBendingLinesBuilderReferencePlaneType
-
class
NXOpen.Features.ShipDesign.
InverseBendingLinesBuilderReferencePlaneType
¶ Bases:
object
The reference plane to draw the diagram on.
Enum Members
Enum Member Enum Member Description XCYCPlane XC-YC plane. YCZCPlane YC-ZC plane. ZCXCPlane ZC-XC plane. NegativeXCYCPlane -XC-YC plane. NegativeYCZCPlane -YC-ZC plane. NegativeZCXCPlane -ZC-XC plane. DefineCSYS User defined plane. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-