InverseBendingLinesBuilderMethodType Enumeration¶
NXOpen.Features.ShipDesign.InverseBendingLinesBuilder.MethodType is an alias for NXOpen.Features.ShipDesign.InverseBendingLinesBuilderMethodType
-
class
NXOpen.Features.ShipDesign.
InverseBendingLinesBuilderMethodType
¶ Bases:
object
The method used to generate the bending curves.
Enum Members
Enum Member Enum Member Description Automatic Automatic. NumberOfCurves Number of curves. FillingCoefficient Filling Coefficient (unsupported). EvenFit Even Fit. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-