GeneralArrangementViewBuilderInheritedPMISourceOption Enumeration¶
NXOpen.Features.ShipDesign.GeneralArrangementViewBuilder.InheritedPMISourceOption is an alias for NXOpen.Features.ShipDesign.GeneralArrangementViewBuilderInheritedPMISourceOption
-
class
NXOpen.Features.ShipDesign.
GeneralArrangementViewBuilderInheritedPMISourceOption
¶ Bases:
object
Settings to indicate the Inherited PMI source type
Enum Members
Enum Member Enum Member Description NoChange do nothing about PMI, this option only work when edit genearl arrangement view NotSet FromGARoot Copy PMI label from General Arrangement Root part FromGAContainer Copy PMI label from General Arrangement Deck Container FromGADrawing Copy PMI label from General Arrangement Drawing Root part FromSourcePart Copy PMI label from the selected source part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-