FeaturesBatchOperationBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
FeaturesBatchOperationBuilder
¶ Bases:
NXOpen.Builder
Use this to cycle through the assembly components and perform the operation globally on the specified feature type.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateFeaturesBatchOperationBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Type | Returns or sets the operation type |
Methods¶
Method | Description |
---|---|
AddFeatureType | Add feature type |
ClearFeatureTypes | Clear feature types |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FeaturesBatchOperationBuilderTypes Enumeration | The option for which kind of operation will be performed. |
Property Detail¶
Type¶
-
FeaturesBatchOperationBuilder.
Type
¶ Returns or sets the operation type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.ShipDesign.FeaturesBatchOperationBuilderTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.ShipDesign.FeaturesBatchOperationBuilderTypes
) –New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Method Detail¶
AddFeatureType¶
-
FeaturesBatchOperationBuilder.
AddFeatureType
¶ Add feature type
Signature
AddFeatureType(featureType)
Parameters: featureType (str) – New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
ClearFeatureTypes¶
-
FeaturesBatchOperationBuilder.
ClearFeatureTypes
¶ Clear feature types
Signature
ClearFeatureTypes()
New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
FeaturesBatchOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.