ExpansionDrawingBuilderJaExpansiondrawingbuilderMetricScale Enumeration¶
NXOpen.Features.ShipDesign.ExpansionDrawingBuilder.JaExpansiondrawingbuilderMetricScale is an alias for NXOpen.Features.ShipDesign.ExpansionDrawingBuilderJaExpansiondrawingbuilderMetricScale
-
class
NXOpen.Features.ShipDesign.
ExpansionDrawingBuilderJaExpansiondrawingbuilderMetricScale
¶ Bases:
object
the standard Metric drawing sheet scales
Enum Members
Enum Member Enum Member Description S501 a scale of 50:1 S201 a scale of 20:1 S101 a scale of 10:1 S51 a scale of 5:1 S21 a scale of 2:1 S11 a scale of 1:1 S12 a scale of 1:2 S15 a scale of 1:5 S110 a scale of 1:10 S120 a scale of 1:20 S150 a scale of 1:50 S1100 a scale of 1:100 Custom a custom scale Default default scale -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-