EdgeReinforcementBuilderEndCutTypes Enumeration¶
NXOpen.Features.ShipDesign.EdgeReinforcementBuilder.EndCutTypes is an alias for NXOpen.Features.ShipDesign.EdgeReinforcementBuilderEndCutTypes
-
class
NXOpen.Features.ShipDesign.
EdgeReinforcementBuilderEndCutTypes
¶ Bases:
object
Used to specify the type of end cut to be used at the extreme ends of the edge reinforcement system.
Enum Members
Enum Member Enum Member Description Connected FlangeFree Sniped SnipedSquare -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-