EdgeCutBuilderVersionID Enumeration¶
NXOpen.Features.ShipDesign.EdgeCutBuilder.VersionID is an alias for NXOpen.Features.ShipDesign.EdgeCutBuilderVersionID
-
class
NXOpen.Features.ShipDesign.
EdgeCutBuilderVersionID
¶ Bases:
object
version identifiers for the different revisions of the edge cut feature.
Enum Members
Enum Member Enum Member Description Nx85 This feature builder is used to edit an existing NX85 - NX9 edge cut feature. Use: SelectTargetFace and GuideCurve Nx901 This feature builder is used to create or edit an NX901 or beyond feature. Use: PlacementGeometry, PathGeometry, ReferencePoint, ReferenceDirection, and if needed PathReverseDirection -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-