EdgeCutBuilderArraySpacing Enumeration¶
NXOpen.Features.ShipDesign.EdgeCutBuilder.ArraySpacing is an alias for NXOpen.Features.ShipDesign.EdgeCutBuilderArraySpacing
-
class
NXOpen.Features.ShipDesign.
EdgeCutBuilderArraySpacing
¶ Bases:
object
available methods used to define the spacing between the cuts
Enum Members
Enum Member Enum Member Description EvenDistribution Cuts will automatically be spaced evenly along the length of the guide CustomDefined The user can specify a custom amount of space between the cuts -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-