DrawingTemplateBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
DrawingTemplateBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a drawing template selection block
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
TemplateName | Returns or sets the template |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
TemplateName¶
-
DrawingTemplateBuilder.
TemplateName
¶ Returns or sets the template
-------------------------------------
Getter Method
Signature
TemplateName
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemplateName
Parameters: templateName (str) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Method Detail¶
Validate¶
-
DrawingTemplateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.