DrawingPartBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
DrawingPartBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.ShipDesign.DrawingPartBuilder
.This class is used to define a drawing part in Ship Section Drawing command, in this case user can define the drawing part manually as he want. Originally, we use a
NXOpen.Features.ShipDesign.SectionDrawingBuilder
class and a list ofNXOpen.Features.ShipDesign.SectionViewBuilder
and the command will calculate the arrangement (like how many drawing parts/draw sheets need to create and which view in which sheet ) automatically. User can’t define which view in which sheet.In this project we make user has ability to define the arrangement in a tree like Drawing Part1 |- Drawing Sheet1 |-View1 |-View2 |- Drawing Sheet2 |- View3 |- View4 Drawing Part2 | - Drawing Sheet1 |- View5 |- View6
So we add
NXOpen.Features.ShipDesign.DrawingPartBuilder
andNXOpen.Features.ShipDesign.DrawingSheetBuilder
between them and make them has structure as below:NXOpen.Features.ShipDesign.SectionDrawingBuilder
NXOpen.Features.ShipDesign.DrawingPartBuilder
NXOpen.Features.ShipDesign.DrawingSheetBuilder
NXOpen.Features.ShipDesign.SectionViewBuilder
To create a new instance of this class, use
NXOpen.Features.ShipDesign.SectionDrawingBuilder.CreateDrawingPartBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
DrawingName | Returns or sets the drawing name |
DrawingSheetList | Returns the drawing sheet list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateDrawingSheetBuilder | Creates a NXOpen.Features.ShipDesign.DrawingSheetBuilder |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DrawingName¶
-
DrawingPartBuilder.
DrawingName
¶ Returns or sets the drawing name
-------------------------------------
Getter Method
Signature
DrawingName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingName
Parameters: drawingName (str) – New in version NX12.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
DrawingSheetList¶
-
DrawingPartBuilder.
DrawingSheetList
¶ Returns the drawing sheet list
-------------------------------------
Getter Method
Signature
DrawingSheetList
Returns: all drawing sheets in this part Return type: NXOpen.Features.ShipDesign.DrawingSheetBuilderList
New in version NX12.0.0.
License requirements: None.
Method Detail¶
CreateDrawingSheetBuilder¶
-
DrawingPartBuilder.
CreateDrawingSheetBuilder
¶ Creates a
NXOpen.Features.ShipDesign.DrawingSheetBuilder
Signature
CreateDrawingSheetBuilder(drawingSheet)
Parameters: drawingSheet ( NXOpen.Drawings.DrawingSheet
) –Returns: Return type: NXOpen.Features.ShipDesign.DrawingSheetBuilder
New in version NX12.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Validate¶
-
DrawingPartBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.