DrawingAnnotationBuilderAnnotation Enumeration¶
NXOpen.Features.ShipDesign.DrawingAnnotationBuilder.Annotation is an alias for NXOpen.Features.ShipDesign.DrawingAnnotationBuilderAnnotation
-
class
NXOpen.Features.ShipDesign.
DrawingAnnotationBuilderAnnotation
¶ Bases:
object
Settings that indicate how to handle the exsiting annotation in the drawing.
Enum Members
Enum Member Enum Member Description Preserve Delete -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-