DeckListItemBuilderDatumDir Enumeration

NXOpen.Features.ShipDesign.DeckListItemBuilder.DatumDir is an alias for NXOpen.Features.ShipDesign.DeckListItemBuilderDatumDir

class NXOpen.Features.ShipDesign.DeckListItemBuilderDatumDir

Bases: object

Represents the thickening direction.

Enum Members

Enum Member Enum Member Description
Plus
Minus
Neutral
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.