DeckListBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
DeckListBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This builder allows you to define the general arrangement view information.
It represents
NXOpen.Features.ShipDesign.DeckListBuilder
.New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
Add | Adds a deck to creation list |
Remove | Removes a deck from creation list |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Add¶
-
DeckListBuilder.
Add
¶ Adds a deck to creation list
Signature
Add(deck)
Parameters: deck ( NXOpen.Assemblies.Component
) – deck container to create the GA viewNew in version NX12.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Remove¶
-
DeckListBuilder.
Remove
¶ Removes a deck from creation list
Signature
Remove(deck)
Parameters: deck ( NXOpen.Assemblies.Component
) – deck container to create the GA viewNew in version NX12.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Validate¶
-
DeckListBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.