BuiltUpManModeBuilderBuiltUpManModeType Enumeration¶
NXOpen.Features.ShipDesign.BuiltUpManModeBuilder.BuiltUpManModeType is an alias for NXOpen.Features.ShipDesign.BuiltUpManModeBuilderBuiltUpManModeType
-
class
NXOpen.Features.ShipDesign.
BuiltUpManModeBuilderBuiltUpManModeType
¶ Bases:
object
This enum defines the allowable values for the BuiltUp Profile Manufacturing Mode which may be either “Cut To Shape” or “Bend After Join”. See the NX Ship documentation for an explanation of these in terms of the manufacturing process.
Enum Members
Enum Member Enum Member Description CutToShape BendAfterJoin NotSet -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-