BracketBuilderLimitTypes Enumeration¶
NXOpen.Features.ShipDesign.BracketBuilder.LimitTypes is an alias for NXOpen.Features.ShipDesign.BracketBuilderLimitTypes
-
class
NXOpen.Features.ShipDesign.
BracketBuilderLimitTypes
¶ Bases:
object
The limit types.
This option specifies how many limit objects there are.
Enum Members
Enum Member Enum Member Description NoLimit The bracket does not have any limit object OneLimit The bracket has one limit object TwoLimit The bracket has two limit objects ThreeLimit The bracket has three limit objects -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-