BracketBuilderAlignmentTypes Enumeration¶
NXOpen.Features.ShipDesign.BracketBuilder.AlignmentTypes is an alias for NXOpen.Features.ShipDesign.BracketBuilderAlignmentTypes
-
class
NXOpen.Features.ShipDesign.
BracketBuilderAlignmentTypes
¶ Bases:
object
The alignment types.
This option specifies how the bracket is aligned.
Enum Members
Enum Member Enum Member Description DatumPlaneAlignment The bracket molding face is aligned to a datum plane AutoAlignment The bracket molding faces is aligned to stiffener molding face Lapped The bracket is lapped with stiffener -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-