AlongGuideCutBuilderWaterStopOffsetMethod Enumeration¶
NXOpen.Features.ShipDesign.AlongGuideCutBuilder.WaterStopOffsetMethod is an alias for NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod
-
class
NXOpen.Features.ShipDesign.
AlongGuideCutBuilderWaterStopOffsetMethod
¶ Bases:
object
Offset option used to define the placement of the water stop guide cut
Enum Members
Enum Member Enum Member Description Symmetric The left offset and right offset are symmetric Asymmetric The left offset and right offset are asymmetric -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-