ShelfBuilderStepMethod Enumeration

NXOpen.Features.ShelfBuilder.StepMethod is an alias for NXOpen.Features.ShelfBuilderStepMethod

class NXOpen.Features.ShelfBuilderStepMethod

Bases: object

Step Method for Side Face

Enum Members

Enum Member Enum Member Description
Normal
AlignwithReferenceFace
Ramp
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.