ShelfBuilderReferenceType Enumeration

NXOpen.Features.ShelfBuilder.ReferenceType is an alias for NXOpen.Features.ShelfBuilderReferenceType

class NXOpen.Features.ShelfBuilderReferenceType

Bases: object

Type of Reference Object

Enum Members

Enum Member Enum Member Description
Face
DatumPlane
Curve
Point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.