ShelfBuilderDepthMethods Enumeration

NXOpen.Features.ShelfBuilder.DepthMethods is an alias for NXOpen.Features.ShelfBuilderDepthMethods

class NXOpen.Features.ShelfBuilderDepthMethods

Bases: object

Depth Method for Depth Face

Enum Members

Enum Member Enum Member Description
Offset
ToNextWall
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.