SheetmetalManagerTabSweepDir Enumeration¶
-
class
NXOpen.Features.SheetMetal.
SheetmetalManagerTabSweepDir
¶ Bases:
object
This enum is for Tab sweep direction flag. Sweep direction can be along the normal to section or opposite to normal.
Enum Members
Enum Member Enum Member Description Normal Tab sweep direction along normal direction OppositeToNormal Tab sweep direction opposite to normal direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-