SheetmetalManagerFlangeWidthOption Enumeration¶
-
class
NXOpen.Features.SheetMetal.
SheetmetalManagerFlangeWidthOption
¶ Bases:
object
Flange width option
Enum Members
Enum Member Enum Member Description CustomizeWidth customize width FullWidth full width Centred centred AtEnd at end FromBothEnds from both ends FromEnd from end -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-