NormalCutoutBuilderCutTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.NormalCutoutBuilder.CutTypeOptions is an alias for NXOpen.Features.SheetMetal.NormalCutoutBuilderCutTypeOptions
-
class
NXOpen.Features.SheetMetal.
NormalCutoutBuilderCutTypeOptions
¶ Bases:
object
This enum represents the cut type for the normal cutout.
Enum Members
Enum Member Enum Member Description ThicknessCut MidPlaneCut NearestFaceCut -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-