MiterOptionsTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.MiterOptions.TypeOptions is an alias for NXOpen.Features.SheetMetal.MiterOptionsTypeOptions
-
class
NXOpen.Features.SheetMetal.
MiterOptionsTypeOptions
¶ Bases:
object
the miter type options.
Enum Members
Enum Member Enum Member Description NormalToSourceFace mitering is done along the normal to source face NormalToThicknessFace mitering is done along the normal to thickness face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-