MiterOptionsClosedCornerTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.MiterOptions.ClosedCornerTypeOptions is an alias for NXOpen.Features.SheetMetal.MiterOptionsClosedCornerTypeOptions
-
class
NXOpen.Features.SheetMetal.
MiterOptionsClosedCornerTypeOptions
¶ Bases:
object
the closed corner type options.
Enum Members
Enum Member Enum Member Description NotSet Corner is not closed Open corner is open Closed corner is closed completely CircularCutout corner has a circular cutout in it UCutout corner has a U shaped cutout in it VCutout corner has a V shaped cutout in it -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-