GussetBuilderWidthSides Enumeration¶
NXOpen.Features.SheetMetal.GussetBuilder.WidthSides is an alias for NXOpen.Features.SheetMetal.GussetBuilderWidthSides
-
class
NXOpen.Features.SheetMetal.
GussetBuilderWidthSides
¶ Bases:
object
This enum represents the different options for thickening the user defined profile Gusset.
Enum Members
Enum Member Enum Member Description Side1 The Gusset will be created on the side of plane normal of the user defined profile. Side2 The Gusset will be created on the opposite side of the plane normal of the user defined profile. Symmetric The Gusset will be created on both sides of the plane of the user defined profile. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-