GussetBuilderShapes Enumeration¶
NXOpen.Features.SheetMetal.GussetBuilder.Shapes is an alias for NXOpen.Features.SheetMetal.GussetBuilderShapes
-
class
NXOpen.Features.SheetMetal.
GussetBuilderShapes
¶ Bases:
object
This enum represents the two different shapes for Gusset.
Enum Members
Enum Member Enum Member Description Square Specifies a square shape for the Gusset Round Specifies a round shape for the Gusset -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-