FlatSolidBuilderOrientationType Enumeration¶
NXOpen.Features.SheetMetal.FlatSolidBuilder.OrientationType is an alias for NXOpen.Features.SheetMetal.FlatSolidBuilderOrientationType
-
class
NXOpen.Features.SheetMetal.
FlatSolidBuilderOrientationType
¶ Bases:
object
The enum defines how to orient flat solid body.
New in version NX12.0.0.
Enum Members
Enum Member Enum Member Description Default do not orient flat solid body Edge transform flat solid body as per orientation defined by edge Csys transform flat solid body as per orientation defined by CSYS -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-