FeatureProperty Enumeration¶
-
class
NXOpen.Features.SheetMetal.
FeatureProperty
¶ Bases:
object
This is a common enum that comprises of values to be used for various features. All Feature builder APIs will enumerate valid values that can be used for that feature parameter.
Enum Members
Enum Member Enum Member Description IgNullConstant IgLeft IgRight IgSymmetric IgInside IgOutside IgBoth IgNormalSidedummy IgReverseNormalSidedummy IgExtend IgNoextend IgThkinprofileplane IgThkNormalToProfilePlane IgFinite IgTonext IgFromTo IgThroughAll IgThreeHundredAndSixty IgParallelDummy IgAngularDummy IgNormal IgThroughAxis IgSingleEdge IgMultipleEdges IgEdgesByLoop IgEdgesByVertex IgAll IgConcave IgConvex IgStart IgEnd IgLinear IgRadial IgRegularHole IgCounterBoreHole IgCounterSinkHole IgCounterDrillHole IgTappedHole IgTaperedHole IgConstRadiusRound IgVarRadiusRound IgChamfer45degSetback IgChamferAngleSetback IgChamfer2Serbacks IgNone IgTaperByAngle IgTaperByRatio IgClosed IgProfileBasedCrosssection IgEdgeBasedCrosssection IgTangent IgRectangularBendRelief IgFilletBendRelief IgRipBendRelief IgBendOnlyCornerRelief IgBendAndFaceCornerRelief IgRipCornerRelief IgNftype IgEquationType IgPatternMirror IgPatternRectangular IgPatternCircular IgPatternUserDefined IgFromReferenceEnd IgFromNonreferenceEnd IgRndRollAcrossTnagentEdgesOn IgRndRollAcrossTangentEdgesOff IgRndCapAcrossSharpEdges IgRndRollAcrossSharpEdges IgRndRollAlongBlendEdgesOn IgRndRollAlongBlendEdgesOff IgToKepPoint IgFlatten IgAsConstruction IgOffset IgMitreParalletToThickness IgMitreNormalToThickness IgMitreByDist IgMitreByAngle IgMiterRegularCut IgMitreManufacturingCut IgProjectOptionProject IgProjectOptionWrap IgLip IgGroove IgPartingFromPlane IgPartingFromSurface IgPartingFromEdge IgPartingFromCurve IgSplitDraft IgSplitAngle1Right IgSplitAngle1Left IgLouverformedendtype IgLouverlancedendtype IgLouverround IgLouverroundnone IgInsideDimension IgOutsideDimension IgFull IgBend IgAddRound IgNoRound IgCloseFaces IgOverlapFaces IgTreatmentOff IgTreatmentIntersect IgTreatmentCircleCutout IgStepDreat IgShowBoundaries IgRemoveBoundaries IgCornerRound IgNoCornerRound IgNatural IgPeriodic IgRoundAllVertexSetback IgRoundSingleVertexSetback IgRoundVertexEdgeSetback IgRoundSetbackIsAbsolute IgRoundSetbackIsRelative IgCircular IgUshaped IgVshaped IgPunchedEnd IgLancedEnd IgFormedEnd IgSweepAlignParallel IgSweepAlignNormal IgRoundStartVertexEdgeSetback IgRoundEndVertexEdgeSetback IgSubtract IgUnite IgIntersect IgContinuous IgFlangeFulledge IgFlangeCenterOfEdge IgFlangeStartOnEndEdge IgFlangeEndOnEndEdge IgFlangeStartFromEndEdge IgFlangeEndFromEndEdge IgFlangeFromBothEndsOfEdge IgFlangeOffset IgChainedCornerRelief IgTangentInterior IgParallelToPlane IgVbottomDimToFlat IgVbottomDimToV IgTaperDimAtTop IgTaperDimAtBottom IgCounterBoreProfileIsAtTop IgCounterBoreProfileIsAtBottom IgTaperByRlRatio IgRndmiteratCorner IgRndRollAroundCorner IgRndPreserveTopologyon IgRndPreserveTopologyOff IgStepDraftPerpendicular IgExtendBendRelief IgEqualOffset IgUnequalOffset IgThickness IgFacesTouchingCurvesOnly IgCurvesetSeperator IgSideInfosetSeperator IgRegularThread IgStraightPipethread IgTaperedPipethread IgRemoveInternalBoundaries IgRemoveExternalBoundaries IgDeleteFaceheal IgEndcaps IgCurvatureContinuous IgNonsymmetric IgTreatmentDraft IgTreatmentCrown IgCloseCornerNone IgCloseCornerOpen IgCloseCornerClosed IgCloseCornerCircleCutout IgPatternAlongCurve IgPatternMountingBoss IgSmClearanceCutout IgSmMidplaceCutout IgCentermark -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-