EditCornerBuilderCornerReliefTypeOptions Enumeration

NXOpen.Features.SheetMetal.EditCornerBuilder.CornerReliefTypeOptions is an alias for NXOpen.Features.SheetMetal.EditCornerBuilderCornerReliefTypeOptions

class NXOpen.Features.SheetMetal.EditCornerBuilderCornerReliefTypeOptions

Bases: object

This enum specifies the type of relief required at the corner.

Enum Members

Enum Member Enum Member Description
NotSet
CircularCutout
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.