DimpleBuilderSidewallTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.DimpleBuilder.SidewallTypeOptions is an alias for NXOpen.Features.SheetMetal.DimpleBuilderSidewallTypeOptions
-
class
NXOpen.Features.SheetMetal.
DimpleBuilderSidewallTypeOptions
¶ Bases:
object
the side walls material option. This specifies whether the dimple’s outerwalls or the innerwalls coincide with the section outline
Enum Members
Enum Member Enum Member Description Outside the innerface of the dimple side walls coincides with the section outline. Inside the outerface of the dimple side walls coincides with the section outline. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-