DimpleBuilderDimensionTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.DimpleBuilder.DimensionTypeOptions is an alias for NXOpen.Features.SheetMetal.DimpleBuilderDimensionTypeOptions
-
class
NXOpen.Features.SheetMetal.
DimpleBuilderDimensionTypeOptions
¶ Bases:
object
the Dimension options for dimple. This specifies whether the dimple’s depth must be measured from the plane to which the section is attached or from the
Enum Members
Enum Member Enum Member Description Offset the actual depth will be depth plus the thickness of sheet. Full the actual extent distance will be the value specified as depth. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-