ContourFlangeBuilderSweepSideOptions Enumeration¶
NXOpen.Features.SheetMetal.ContourFlangeBuilder.SweepSideOptions is an alias for NXOpen.Features.SheetMetal.ContourFlangeBuilderSweepSideOptions
-
class
NXOpen.Features.SheetMetal.
ContourFlangeBuilderSweepSideOptions
¶ Bases:
object
This enum represents the side in which the contour flange will be swept.
Enum Members
Enum Member Enum Member Description SectionNormalSide SectionReverseNormalSide -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-