ClosedCornerBuilderTreatmentTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.ClosedCornerBuilder.TreatmentTypeOptions is an alias for NXOpen.Features.SheetMetal.ClosedCornerBuilderTreatmentTypeOptions
-
class
NXOpen.Features.SheetMetal.
ClosedCornerBuilderTreatmentTypeOptions
¶ Bases:
object
This enum represents Corner treatment type
Enum Members
Enum Member Enum Member Description Open Only Webs will be closed Closed Bend and Webs will be closed CircularCutout Circular shaped relief UCutout U shaped relief VCutout V shaped relief RectangularCutout Rectangular shaped relief -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-